This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

搬移到RAM中运行



        如果主程序执行是的一个状态机,时序要求比较严格,那么是不是搬移到RAM中执行的会快一点,那么怎么把main的主要代码都搬移到RAM中里面呢?

就是for(;;)之后的代码?

  • 在应用中为了提高关键代码的执行速度,可以通过将Flash中的对应代码搬移到RAM中执行。具体的实现一般分为4步:

    (1)在cmd文件中声明ramfuncs地址空间,包括代码在Load(下载)和Run(执行)时所分别对应的Flash和RAM地址;

    (2)定义代码搬移函数,MemCopy():其主要功能为将Flash所对应的代码搬移至RAM;

    (3)在main.c中首先声明需要搬移的函数,声明三个外部变量,执行MemCopy(),将对应的函数搬移至RAM中;

    (4)在工程中添加以上的操作,便可以正常调用相关函数,该函数会自动跳转至RAM中运行。

     

     

    补充:

    为了有效地提升代码执行速率,建议只将部分关键代码搬移至RAM中运行,没有必要将main()主函数的全部代码搬移至RAM。

  • 您好,请问为什么跑马灯程序在带仿真器时运行比不带仿真器下运行快呢?跑马灯所用的延时程序已经搬移到ram了。

  • 如果程序中的跑马灯是通过定时器中断来实现的话,那么程序运行的快慢还应该与相应的中断响应函数在 RAM 中还是 Flash 中运行有关。

  • 我已经把灯的亮灭在定时中断程序,中断程序放在RAM中运行,可是还是会出当拿掉仿真器后速度会变慢很多,附件中是我的代码,麻烦帮忙看一看

    #include "DSP280x_Device.h" // DSP280x Headerfile Include File
    #include "DSP280x_Examples.h" // DSP280x Examples Include File

    // Configure which ePWM timer interrupts are enabled at the PIE level:
    // 1 = enabled, 0 = disabled
    #define PWM3_INT_ENABLE 1

    // Configure the period for each timer
    #define PWM3_TIMER_TBPRD 0x1FFF

    // Make this long enough so that we can see an LED toggle
    #define DELAY 1000000L
    #define DELAY1 100000L

    // Functions that will be run from RAM need to be assigned to
    // a different section. This section will then be mapped using
    // the linker cmd file.
    #pragma CODE_SECTION(epwm3_timer_isr, "ramfuncs");
    // Prototype statements for functions found within this file.

    interrupt void epwm3_timer_isr(void);
    void InitEPwmTimer(void);
    void Gpio_select(void);
    // Global variables used in this example
    Uint32 EPwm1TimerIntCount;
    Uint32 EPwm2TimerIntCount;
    Uint32 EPwm3TimerIntCount;
    Uint32 LoopCount;

    // These are defined by the linker (see F2808.cmd)
    extern Uint16 RamfuncsLoadStart;
    extern Uint16 RamfuncsLoadEnd;
    extern Uint16 RamfuncsRunStart;

    void main(void)
    {

    // Step 1. Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    // This example function is found in the DSP280x_SysCtrl.c file.
    InitSysCtrl();

    // Step 2. Initalize GPIO:
    // This example function is found in the DSP280x_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    // InitGpio(); // Skipped for this example
    EALLOW;
    GpioCtrlRegs.GPAMUX1.all = 0x0; // GPIO pin
    GpioCtrlRegs.GPADIR.all = 0xFF; // Output pin
    GpioDataRegs.GPADAT.all =0xFF; // Close LEDs
    EDIS;

    // For this example use the following configuration:
    Gpio_select();

    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
    DINT;

    // Initialize the PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the DSP280x_PieCtrl.c file.
    InitPieCtrl();

    // Disable CPU interrupts and clear all CPU interrupt flags:
    IER = 0x0000;
    IFR = 0x0000;

    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example. This is useful for debug purposes.
    // The shell ISR routines are found in DSP280x_DefaultIsr.c.
    // This function is found in DSP280x_PieVect.c.
    InitPieVectTable();

    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
    EALLOW; // This is needed to write to EALLOW protected registers
    // PieVectTable.EPWM1_INT = &epwm1_timer_isr;
    // PieVectTable.EPWM2_INT = &epwm2_timer_isr;
    PieVectTable.EPWM3_INT = &epwm3_timer_isr;
    EDIS; // This is needed to disable write to EALLOW protected registers

    // Step 4. Initialize all the Device Peripherals:
    // This function is found in DSP280x_InitPeripherals.c
    // InitPeripherals(); // Not required for this example
    InitEPwmTimer(); // For this example, only initialize the ePWM Timers
    MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);

    // Call Flash Initialization to setup flash waitstates
    // This function must reside in RAM
    InitFlash();

    // Initalize counters:
    EPwm1TimerIntCount = 0;
    EPwm2TimerIntCount = 0;
    EPwm3TimerIntCount = 0;
    LoopCount = 0;

    // Enable CPU INT3 which is connected to EPWM1-3 INT:
    IER |= M_INT3;

    // Enable EPWM INTn in the PIE: Group 3 interrupt 1-3
    PieCtrlRegs.PIEIER3.bit.INTx3 = PWM3_INT_ENABLE;

    // Enable global Interrupts and higher priority real-time debug events:
    EINT; // Enable Global interrupt INTM
    ERTM; // Enable Global realtime interrupt DBGM

    // Step 6. IDLE loop. Just sit and loop forever (optional):
    EALLOW;
    GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0;
    GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;
    EDIS;

    for(;;)
    {
    // This loop will be interrupted, so the overall
    // delay between pin toggles will be longer.
    DELAY_US(DELAY);
    LoopCount++;
    GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1;
    }

    }


    void InitEPwmTimer()
    {

    EALLOW;
    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; // Stop all the TB clocks
    EDIS;

    // Setup Sync
    EPwm3Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through
    // Allow each timer to be sync'ed
    EPwm3Regs.TBCTL.bit.PHSEN = TB_ENABLE;
    EPwm3Regs.TBPHS.half.TBPHS = 300;
    EPwm3Regs.TBPRD = PWM3_TIMER_TBPRD;
    EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up
    EPwm3Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Enable INT on Zero event
    EPwm3Regs.ETSEL.bit.INTEN = PWM3_INT_ENABLE; // Enable INT
    EPwm3Regs.ETPS.bit.INTPRD = ET_3RD; // Generate INT on 3rd event

    EALLOW;
    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; // Start all the timers synced
    EDIS;


    }


    interrupt void epwm3_timer_isr(void)
    {
    Uint16 i;

    EPwm3TimerIntCount++;

    // Short Delay to simulate some ISR Code
    for(i = 1; i < 0x01FF; i++) {}
    GpioDataRegs.GPADAT.all=0xFFFDFFFF; //GPIO17=0 LED灯亮
    DELAY_US(DELAY1);
    GpioDataRegs.GPADAT.all=0xFFF7FFFF; //GPIO19=0
    DELAY_US(DELAY1);
    // Clear INT flag for this timer
    EPwm3Regs.ETCLR.bit.INT = 1;

    // Acknowledge this interrupt to receive more interrupts from group 3
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
    }

    void Gpio_select(void)
    {


    EALLOW;

    GpioCtrlRegs.GPAPUD.bit.GPIO6 = 0; // Enable pullup on GPIO11
    GpioDataRegs.GPASET.bit.GPIO6 = 1; // Load output latch
    GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 0; // GPIO11 = GPIO
    GpioCtrlRegs.GPADIR.bit.GPIO6 = 1; // GPIO11 = output

    GpioCtrlRegs.GPAPUD.bit.GPIO16= 0; // Enable pullup on GPIO11
    GpioDataRegs.GPASET.bit.GPIO16 = 1; // Load output latch
    GpioCtrlRegs.GPAMUX2.bit.GPIO16 = 0; // GPIO11 = GPIO
    GpioCtrlRegs.GPADIR.bit.GPIO16 = 1; // GPIO11 = output

    GpioCtrlRegs.GPAPUD.bit.GPIO17 = 0; // Enable pullup on GPIO11
    GpioDataRegs.GPASET.bit.GPIO17 = 1; // Load output latch
    GpioCtrlRegs.GPAMUX2.bit.GPIO17 = 0; // GPIO11 = GPIO
    GpioCtrlRegs.GPADIR.bit.GPIO17 = 1; // GPIO11 = output

    GpioCtrlRegs.GPAPUD.bit.GPIO19 = 0; // Enable pullup on GPIO11
    GpioDataRegs.GPASET.bit.GPIO19 = 1; // Load output latch
    GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 0; // GPIO11 = GPIO
    GpioCtrlRegs.GPADIR.bit.GPIO19= 1; // GPIO11 = output

    GpioCtrlRegs.GPAPUD.bit.GPIO8 = 0; // Enable pullup on GPIO11
    GpioDataRegs.GPASET.bit.GPIO8 = 1; // Load output latch
    GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 0; // GPIO11 = GPIO
    GpioCtrlRegs.GPADIR.bit.GPIO8 = 1; // GPIO11 = output

    GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 0; // GPIO11 = GPIO
    GpioCtrlRegs.GPADIR.bit.GPIO31 = 0; // GPIO11 = output

    EDIS;

    }