This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP28335— DELAY_US总结

在很多程序中都会调用延时程序DELAY_US(A),在文件DSP281x_Examples.h中有如下宏定义:
#define DELAY_US(A) DSP28x_usDelay(((((long double) A * 1000.0L) / (long double)CPU_RATE) - 9.0L) / 5.0L)

从定义很容易推算出,需要延时A微妙就把DELAY_US()的参数设置为A即可。

在仿真调试的情况下运行程序,延时是较准确的,但是当把程序烧写到flash里运行时,如果程序上不做修改,就会很容易发现延时的时间比你设置的要长(通过延时控制LED灯闪烁,很直观)。这是因为,DSP访问flash时需要等待时间的,而访问RAM时几乎是零等待,所以在使用DELAY_US(A)时要想延时时间准确必须使其在RAM里运行,在程序上需做如下修改:

1、在DSP2833x_usDelay.asm中,有如下代码:


       .def _DSP28x_usDelay
       .sect "ramfuncs"

        .global  __DSP28x_usDelay
_DSP28x_usDelay:
        SUB    ACC,#1
        BF     _DSP28x_usDelay,GEQ    ;; Loop if ACC >= 0
        LRETR

其中.sect "ramfuncs"语句的作用就是就把用汇编写的函数DSP28x_usDelay定位在ramfuncs段。

2、在工程中添加源文件DSP2833x_MemCopy.c,该文件中的函数void MemCopy(Uint16 *SourceAddr, Uint16* SourceEndAddr, Uint16* DestAddr),实现把你想复制的代码从装载地址RamfuncsLoadStart—RamfuncsLoadEnd拷贝到RamfuncsRunStart开始的SARAM空间中。

 

3、在文件DSP2833x_SysCtrl.c开头,通过伪指令定义一个代码段,注意位置一定要放在函数前面(如下图所示)。

4、在main函数中要调用MemCopy函数,注意该函数放置的位置。

5、修改用于烧写的CMD文件

6、注意在头文件DSP281x_GlobalPrototypes.h 别忘做如下声明:

 

  • 麻烦请问延时函数的程序#define DELAY_US(A) DSP28x_usDelay(((((long double) A * 1000.0L) / (long double)CPU_RATE) - 9.0L) / 5.0L)适用的晶振主频是多少?   如果是150M的晶振应该怎么修改? 多谢