This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

memcopy跟memcpy

memcopy没有问题。 memcopy跟memcpy是不一样的。

void MemCopy(Uint16 *SourceAddr, Uint16* SourceEndAddr, Uint16* DestAddr)

 {    

while(SourceAddr < SourceEndAddr)    

 {   

     *DestAddr++ = *SourceAddr++;    

 }    

 return;

 }

void* memcpy(void*destaddr,voidconst*srcaddr,size_tlen)

{

    char* dest=destaddr;

    char const* src=srcaddr;

    while(len-->0)

    {

    *dest++ = *src++;

    }

    return destaddr;

}

 ramfuncs   : LOAD = FLASHD, 
                         RUN = RAML0, 
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         PAGE = 0

第1行表示该段的装载在PAGA0的FLASHD中
第2行表示该段的运行地址在PAGE0的RAML0中
LOAD_ START(_RamfuncsLoadStart)令编译器创建了一个变量RamfuncsLoadStart,该变量指向段ramfuncs的装载地址的首地址(LOAD_ START为编译伪指令,请见CCS的帮助文档);
LOAD_ START(_RamfuncsLoadEnd)令编译器创建了一个变量RamfuncsLoadEnd,该变量指向段ramfuncs的装载地址的末地址(LOAD_ END为编译伪指令,请见CCS的帮助文档);
LOAD_ START(_RamfuncsRunStart)令编译器创建了一个变量RamfuncsRunStart,该变量指向段ramfuncs的运行地址的首地址(LOAD_ START为编译伪指令,请见CCS的帮助文档);
从第1和2行可以看出,段ramfuncs中的函数DSP28x_usDelay()的装载地址和运行地址是不同的,本程序中装载在Flash的块FLASHD中,而在SARAM L0中运行,这只是目标,实际运行时DSP并不会自动将Flash中的代码拷贝到SARAM中,因此需要手动添加代码来完成。
在C函数中,为了使用变量RamfuncsLoadStart、RamfuncsLoadEnd和RamfuncsRunStart,必须先声明,本工程在文件DSP2833x_GlobalPrototypes.h中做了如下声明:
extern Uint16 RamfuncsLoadStart;
extern Uint16 RamfuncsLoadEnd;
extern Uint16 RamfuncsRunStart;
然后就可以使用了。在Main.c中,使用MemCopy()函数将段ramfuncs中的函数DSP28x_usDelay()的代码从装载地址RamfuncsLoadStart—RamfuncsLoadEnd拷贝到RamfuncsRunStart开始的SARAM空间中。之后在程序运行时,只要调用DSP28x_usDelay()函数,都会自动地指向SARAM中相应的函数入口地址,这一点是自动完成的。MemCopy()函数原型在MemCopy.c中,DSP2833x_GlobalPrototypes.h声明。