看了看技术文档,发现有些地方不太理解。(刚开始学,有点艰难)希望懂的人帮忙解答一下,非常感谢!
(1)Each output unit has eight operating modes that generate signals based on the
EQU0 and EQUn signals,我想问一下EQU0和EQUn,是怎么影响输出的?
(2)EQU0和EQUn的值是根据什么条件怎样变化的?
(3)输出模式0的时候:The output signal OUTn is defined by the OUT bit.The OUTn signal updates immediately
when OUT is updated.这个时候OUT是哪来的,或者再问的大一点,OUT位是根据什么条件怎样变化的?
(4)OUTn最开始是低电平还是高电平?比如说我想用翻转模式产生PWM波,如果最开始电平搞反了,很可能占空比就会相反。我的担心是不是多余的啊?