This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
等间隔AD采样
本测试为系列测试的第二个测试,等间隔AD采样测试。
本次测试为等间隔采样测试,其基本设计想法是,通过TIMER A的比较输出产生一个等间隔的AD转换信号,触发AD定时完成AD转换动作,并记录转换结果,通过uart展示AD转换结果。
产生的转换信号频率为128次/20ms,单次转换时间为156.25us。采用P55作为模拟量输入引脚。如下图开发板引脚定义中A0-P5.5。
开发板引脚定义:
初始化系统工作于48MHz,同时调整MCLK为HFXT时钟源,SMCLK采用内部DCO时钟(3MHz)。
CS_setDCOCenteredFrequency(CS_DCO_FREQUENCY_48); CS_initClockSignal(CS_MCLK, CS_HFXTCLK_SELECT, CS_CLOCK_DIVIDER_1 ); CS_initClockSignal(CS_HSMCLK, CS_HFXTCLK_SELECT, CS_CLOCK_DIVIDER_2 ); CS_initClockSignal(CS_SMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1 ); CS_initClockSignal(CS_ACLK, CS_REFOCLK_SELECT, CS_CLOCK_DIVIDER_1 );
这里必须强调一句,必须将Flash的等待延时设置为3以上
/* Set 2 flash wait states for Flash bank 0 and 1*/ FlashCtl_setWaitState(FLASH_BANK0, 3); FlashCtl_setWaitState(FLASH_BANK1, 3);
之前的调试这个值设置为2,总是不正确,改为3后系统可以真确运行了。依据MSP432P401R的数据手册中的相关说明,如下表所示,48Mhz时对应flash wait states为3.
由于转换速度较快,因此初始化ADC的时钟为MCLK,4分频24MHz。ADC可以工作的最高频率为25MHz。
ADC14_initModule(ADC_CLOCKSOURCE_MCLK, ADC_PREDIVIDER_1, ADC_DIVIDER_4, 0);
选用TIMER A0 的CCR1和CCR0构成的比较输出作为ADC的转换控制信号。
从用户手册中我们可以看到ADC14SHSx可以有8种采样控制输入源。
从数据手册中可以找到ADC的外部触发源信号,如下表所示,001对应TA0_C1的比较输出信号。这个信号是准备选用的采样控制信号。
函数,设置触发源1:
ADC14_setSampleHoldTrigger(ADC_TRIGGER_SOURCE1, false);
初始化定时器,由于希望定时周期为156.25us产生一次触发信号,因此,定时器的周期为156.25us
选用SMCLK作为定时器的时钟源,3分频后,定时器的实际计数频率为1MHz。
可得周期值为v = 156.25us*1M*10-6 = 163.84≈164 。因此设置CCR0 = 164.
比较输出CCR1的比较值选择CCR0的1半,同时设置比较数据为set/reset模式。
定时器的设置为:
/* Timer_A Continuous Mode Configuration Parameter */ const Timer_A_UpModeConfig upModeConfig = { TIMER_A_CLOCKSOURCE_SMCLK, // SMCLK Clock Source TIMER_A_CLOCKSOURCE_DIVIDER_3, // SMCLK/1 = 1Mhz 164, TIMER_A_TAIE_INTERRUPT_DISABLE, // Disable Timer ISR TIMER_A_CCIE_CCR0_INTERRUPT_DISABLE, // Disable CCR0 TIMER_A_DO_CLEAR // Clear Counter }; /* Timer_A Compare Configuration Parameter */ const Timer_A_CompareModeConfig compareConfig = { TIMER_A_CAPTURECOMPARE_REGISTER_1, // Use CCR1 TIMER_A_CAPTURECOMPARE_INTERRUPT_DISABLE, // Disable CCR interrupt TIMER_A_OUTPUTMODE_SET_RESET, // Toggle output but 82 // };
将A0接3.3V,读数应该接近最大值16384;将A0接GND,读数应该为0.