代码工程来自于github,工程的介绍如下所示:
IOT Work with TIVA TM4C
In this work you can find out an IOT implementation with TI TivaWare TM4C board.
http_get.c is the main code which you have to execute.
What this program do?
First of all this program is suitable for Code Composer Studio platform.It's written in CCS 9.2.0 , please be careful about this matter.
This program aiming to creating a system which requirements listed as below ;
-Program has to be a timer.This timer trigger the semaphore every 15 seconds to executing the next task.
-First task is TaskForTMP006 , this task pending for semaphore0.Semaphore0 sending by TimerISR.
-TaskForTMP006 created for getting temperature value from tmp006 sensor.
-Second task is TaskForBMP180 , this task pending for semaphore1.Semaphore1 sending by TaskForTMP006.
-TaskForBMP180 created for getting pressure value from BMP180 sensor.
-This sensors available on BOOSTXL SENSHUB.If you have not this part , this program couldn't work.
-To get the temperature and pressure values from the internet , system use the ethernet connection.So , you have to connect the Tiva tm4c1294ncpdt's port with the Wi-Fi modem's LAN port.
To get more information about usage of program please contact me. fhg971 at gmail dot com