再請教一下
如果CAN的TX和RX腳位對接,可以以這樣測試發送和接收數據嗎?
還是一定要接CAN transceiver才有辦法測試呢?
謝謝
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Susan
目前是使用開發版TM4C1294XL Rev D
一塊開發版測試CAN0與CAN1發送與接收測試
一開始就有提到沒有接transceiver測試
無量測CAN引脚的波形
#include "CANFunctions.h" extern uint32_t g_ui32SysClock; volatile uint8_t CAN0ErrFlag = 0; volatile uint8_t CAN1ErrFlag = 0; tCANMsgObject CAN0RxMsgObject,CAN0TxMsgObject; //CAN0 have32 objects tCANMsgObject CAN1RxMsgObject,CAN1TxMsgObject; //CAN1 have32 objects uint8_t CAN0_Obj1RxData[8],CAN0_Obj2RxData[8],CAN0_Obj3RxData[8]; uint8_t CAN1_Obj1RxData[8],CAN1_Obj2RxData[8],CAN1_Obj3RxData[8]; uint8_t CAN0_Obj1TxData[8],CAN1_Obj1TxData[8]; volatile bool CAN0TxMsgObj4Sent = 0; volatile bool CAN1TxMsgObj4Sent = 0; void CAN0IntHandler(void) { uint32_t ui32Status; // // Read the CAN interrupt status to find the cause of the interrupt // ui32Status = CANIntStatus(CAN0_BASE, CAN_INT_STS_CAUSE); // // If the cause is a controller status interrupt, then get the status // if(ui32Status == CAN_INT_INTID_STATUS) { // // Read the controller status. This will return a field of status // error bits that can indicate various errors. Error processing // is not done in this example for simplicity. Refer to the // API documentation for details about the error status bits. // The act of reading this status will clear the interrupt. // ui32Status = CANStatusGet(CAN0_BASE, CAN_STS_CONTROL); CAN0ErrFlag++; } // // Check if the cause is message object 1. // else if(ui32Status == 1) { CANIntClear(CAN0_BASE, ui32Status); CAN0RxMsgObject.pui8MsgData = CAN0_Obj1RxData; CANMessageGet(CAN0_BASE, ui32Status, &CAN0RxMsgObject, 0); CAN0ErrFlag = 0; } // // Check if the cause is message object 2. // else if(ui32Status == 2) { CANIntClear(CAN0_BASE, ui32Status); CAN0RxMsgObject.pui8MsgData = CAN0_Obj2RxData; CANMessageGet(CAN0_BASE, ui32Status, &CAN0RxMsgObject, 0); CAN0ErrFlag = 0; } // // Check if the cause is message object 3. // else if(ui32Status == 3) { CANIntClear(CAN0_BASE, ui32Status); CAN0RxMsgObject.pui8MsgData = CAN0_Obj3RxData; CANMessageGet(CAN0_BASE, ui32Status, &CAN0RxMsgObject, 0); CAN0ErrFlag = 0; } // Check if the cause is message object 4, which is used for sending messages. else if(ui32Status == 4) { CANIntClear(CAN0_BASE, ui32Status); CAN0TxMsgObj4Sent = 1; CAN0ErrFlag = 0; } } void CAN1IntHandler(void) { uint32_t ui32Status; // // Read the CAN interrupt status to find the cause of the interrupt // ui32Status = CANIntStatus(CAN1_BASE, CAN_INT_STS_CAUSE); // // If the cause is a controller status interrupt, then get the status // if(ui32Status == CAN_INT_INTID_STATUS) { // // Read the controller status. This will return a field of status // error bits that can indicate various errors. Error processing // is not done in this example for simplicity. Refer to the // API documentation for details about the error status bits. // The act of reading this status will clear the interrupt. // ui32Status = CANStatusGet(CAN1_BASE, CAN_STS_CONTROL); CAN1ErrFlag++; } // // Check if the cause is message object 1. // else if(ui32Status == 1) { CANIntClear(CAN1_BASE, 1); CAN1RxMsgObject.pui8MsgData = CAN1_Obj1RxData; CANMessageGet(CAN0_BASE, ui32Status, &CAN1RxMsgObject, 0); CAN1ErrFlag = 0; } // // Check if the cause is message object 2. // else if(ui32Status == 2) { CANIntClear(CAN1_BASE, 2); CAN1RxMsgObject.pui8MsgData = CAN1_Obj2RxData; CANMessageGet(CAN0_BASE, ui32Status, &CAN1RxMsgObject, 0); CAN1ErrFlag = 0; } // // Check if the cause is message object 3. // else if(ui32Status == 3) { CANIntClear(CAN1_BASE, 3); CAN1RxMsgObject.pui8MsgData = CAN1_Obj3RxData; CANMessageGet(CAN0_BASE, ui32Status, &CAN1RxMsgObject, 0); CAN1ErrFlag = 0; } // Check if the cause is message object 4, which is used for sending messages. else if(ui32Status == 4) { CANIntClear(CAN1_BASE, ui32Status); CAN1TxMsgObj4Sent = 1; CAN1ErrFlag = 0; } } void CAN0RXConfig(uint8_t ObjNum,uint32_t MsgID) { // Initialize a message object to receive CAN messages with ID 0x1001. // The expected ID must be set along with the mask to indicate that all // bits in the ID must match. // CAN0RxMsgObject.ui32MsgID = MsgID; CAN0RxMsgObject.ui32MsgIDMask = 0xfffff; CAN0RxMsgObject.ui32Flags = (MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER | MSG_OBJ_EXTENDED_ID); CAN0RxMsgObject.ui32MsgLen = 8; // Now load the message object into the CAN peripheral message object 1. // Once loaded the CAN will receive any messages with this CAN ID into // this message object, and an interrupt will occur. // CANMessageSet(CAN0_BASE, ObjNum, &CAN0RxMsgObject, MSG_OBJ_TYPE_RX); } void CAN1RXConfig(uint8_t ObjNum,uint32_t MsgID) { // Initialize a message object to receive CAN messages with ID 0x1001. // The expected ID must be set along with the mask to indicate that all // bits in the ID must match. // CAN1RxMsgObject.ui32MsgID = MsgID; CAN1RxMsgObject.ui32MsgIDMask = 0xfffff; CAN1RxMsgObject.ui32Flags = (MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER | MSG_OBJ_EXTENDED_ID); CAN1RxMsgObject.ui32MsgLen = 8; // Now load the message object into the CAN peripheral message object 1. // Once loaded the CAN will receive any messages with this CAN ID into // this message object, and an interrupt will occur. // CANMessageSet(CAN0_BASE, ObjNum, &CAN1RxMsgObject, MSG_OBJ_TYPE_RX); } void CANMultiRXConfig() { CAN0RXConfig(1,0x1001); CAN0RXConfig(2,0x1002); CAN0RXConfig(3,0x1003); CAN1RXConfig(1,0x2001); CAN1RXConfig(2,0x2002); CAN1RXConfig(3,0x2003); } void CAN0TXSend(uint8_t ObjNum,uint32_t MsgID) { CAN0TxMsgObject.ui32MsgID = MsgID; CAN0TxMsgObject.ui32MsgIDMask = 0; CAN0TxMsgObject.ui32Flags = MSG_OBJ_TX_INT_ENABLE; CAN0TxMsgObject.ui32MsgLen = sizeof(CAN0_Obj1TxData); CAN0_Obj1TxData[0]++; CAN0TxMsgObject.pui8MsgData = CAN0_Obj1TxData; CAN0TxMsgObj4Sent=0; CANMessageSet(CAN0_BASE, ObjNum, &CAN0TxMsgObject, MSG_OBJ_TYPE_TX); } void CAN1TXSend(uint8_t ObjNum,uint32_t MsgID) { CAN1TxMsgObject.ui32MsgID = MsgID; CAN1TxMsgObject.ui32MsgIDMask = 0; CAN1TxMsgObject.ui32Flags = MSG_OBJ_TX_INT_ENABLE; CAN1TxMsgObject.ui32MsgLen = sizeof(CAN1_Obj1TxData); CAN1_Obj1TxData[0]++; CAN1TxMsgObject.pui8MsgData = CAN1_Obj1TxData; CAN1TxMsgObj4Sent=0; CANMessageSet(CAN1_BASE, ObjNum, &CAN1TxMsgObject, MSG_OBJ_TYPE_TX); } void CANInitial(void) { SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN0); // The GPIO port and pins have been set up for CAN. The CAN peripheral must be enabled. CANInit(CAN0_BASE); // Initialize the CAN controller CANBitRateSet(CAN0_BASE, g_ui32SysClock, 1000000u); // Set up the 1M bit rate for the CAN bus. //HWREG(CAN0_BASE+CAN_O_CTL) |= CAN_CTL_TEST; //HWREG(CAN0_BASE+CAN_O_TST) |= CAN_TST_LBACK; //CANIntRegister(CAN0_BASE, CAN0IntHandler); // if using dynamic vectors CANIntEnable(CAN0_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS); IntEnable(INT_CAN0);// Enable the CAN interrupt on the processor (NVIC). CANEnable(CAN0_BASE);// Enable the CAN for operation. SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN1); // The GPIO port and pins have been set up for CAN. The CAN peripheral must be enabled. CANInit(CAN1_BASE); // Initialize the CAN controller CANBitRateSet(CAN1_BASE, g_ui32SysClock, 1000000u); // Set up the 1M bit rate for the CAN bus. //CANIntRegister(CAN1_BASE, CAN1IntHandler); // if using dynamic vectors CANIntEnable(CAN1_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS); IntEnable(INT_CAN1);// Enable the CAN interrupt on the processor (NVIC). CANEnable(CAN1_BASE);// Enable the CAN for operation. CANMultiRXConfig(); }