This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540 在嵌入式Linux的驱动开发

Other Parts Discussed in Thread: CC2540, CC2640

我们开发的设备主控制器芯片是TI的DM368,蓝牙芯片打算使用CC2540,两者通过UART相连,通过CC2540连接其他蓝牙设备,获取数据给主处理器DM368,有几个问题想问下大家:

1. CC2540芯片出厂应该没有Fireware,都需要我们烧入镜像的吧?

2. 我们这个系统的CC2540应该是运行Network Processor模式(非Single device模式),所以烧入的镜像应该是HostTestRelease的hex?

3. 当CC2540处于NetWork Processor模式下,在windows下有BTool工具发现设备,连接设备等一些操作。

    如果是DM368这种嵌入式Linux环境下了,是否需要添加对应的driver,是不是Linux内核自带的蓝牙驱动就可以了,另外应用层工具是不是hciconfig ,hcitool就     可以满足了,总之就是在主控制芯片这端还需要什么开发工作?

4. 另外如果就把CC2540运行于Single deivice模式,蓝牙application和Profile都运行在CC2540上,将获取到的数据直接通过串口发生给主控制器DM368,这种方式是不是也可以,且开发的工作量相对于上面那种方式小。

第一次接触蓝牙开发,可能有些没有说清楚,先谢谢大家。