This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530的天线如何设计,另外在画PCB原理图和PCB板子的时候怎么做?

Other Parts Discussed in Thread: CC2530, CC2530EM, CC2531USB-RD

我不懂啊,求高手给个参考。我正画PCB板子呢,忙一天了,终于官方给的参考电路画完了,就剩天线不知道怎么弄了,求前辈指定,或者干脆给个你做的文档看看。

  • CC2530有参考设计,完全参照。从IC RF_N,RF_P到balun到匹配线到天线,尽量接近TI的参考设计,板厚,板材等在参考设计的readme.txt中有。器件的选型,摆放的方向也要按照TI的设计。讲理论一堆的理论。一句话,照着参考设计画,不要搞创意,应该都不会差。

    大尺寸天线

    http://www.ti.com/tool/cc2530em

    小尺寸天线

    http://www.ti.com/tool/cc2531usb-rd

    设计注意事项

    Below is some additional notes when you are copying TI Reference design.

     

    Understand the PCB board properties

    –        PCB stack-up

    –        PCB board dielectric properties (dielectric constant and loss tangent).

    –        TI reference designs include a document describing above properties Readme.txt

     

    The checklist below provides important RF PCB design considerations to be followed

     

    1. Verify the stack-up matches the reference design. If the design is a 4-layer PCB; verify that ground plane is layer two right below top/component side.
    2. Changing the layer spacing/stack-up will affect the matching in the RF signal path and should be carefully accounted for as explained in AN068
    3. Ensure that you follow the datasheet layout recommendation unique to the part (CCXXXX).
    4.  0603(mills) discrete parts are not recommended because of size and parasitic values.
    5. Verify that bypassing/decoupling capacitors are as close as possible to the power supply pins that they are meant to bypass/decouple.
    6. Ensure each decoupling capacitor only decouples the specific pins recommended on the reference design and that the capacitor is correct value and type.
    7. Ensure that decoupling is done pin<>capacitor<>via.
    1. Verify that the ground plane matches the reference design.  There should be a solid ground plane below the device and the RF path. 
    2. Verify that RF signal path matches the reference design as closely as possible. Components should be arranged in a very similar way and oriented the same as the reference design.
    3. The crystal oscillator should be as close as possible to the oscillator pins of the part. Long lines to the oscillator should be avoided if possible.
    4. Verify that the top ground planes are stitched to the ground plane layer and bottom layer with many vias around the RF signal path.  Compare to the reference design.  Vias on the rest of the board should be no more than l/10 apart.
    5. If the part has differential output, ensure that the traces in the differential section and differential section are symmetrical as in the reference design.
    6. If the design uses a battery (such as a coin cell), the battery will act as a ground plane and should therefore not be placed under the antenna.
    7. If the reference design specifies using T-Lines (Transmission Lines), it is very critical to ensure that the T-Lines match the reference design exactly.
    1. Verify that the under-the-device power pad layout is correct. The solder pads and mask should match and the opening size should ensure correct amount of paste. Vias should be the correct number and masked/tented to ensure that they don’t suck up all the solder, leaving none to solder the chip to pad. (Refer to the datasheet for the recommended layout for the corresponding part)
    2. The board should specify impedance controlled traces. That is, the layer spacing and FR4 permittivity should be controlled and known.

     

    Important considerations for Antennas

    1. If using an antenna from a TI reference design, be sure to copy the design exactly as drawn and check if the stack-up in the reference design matches your stack-up.
    2. Changes to feed line length of antenna will change input impedance match.
    3. PCB and chip antennas should not have any ground plane under them.
    4. Any metal in close proximity, plastic enclosure, and human body will change the antennas input impedance and resonance frequency, which must be considered in the design.
    5. For multiple antenna on same board, use antenna polarization and directivity to isolate.
    6. For chip antennas verify that the spacing from and orientation with respect to the ground plane is correct as specified in their datasheet.

     

     

  • 那个参考设计的pcb用那个软件打开呢

  • 建议用CADSTAR打开,也可以用AD打开

  • 好的谢谢你的回复,已经打开了

  • 你好,请问PCB天线在生产的时候需要注意哪些事项呢?PCB天线需要特殊工艺处理吗?

  • 你好,请问PCB天线在生产的时候需要注意哪些事项呢?PCB天线需要特殊工艺处理吗?

  • 你好,请问PCB天线在生产的时候需要注意哪些事项呢?PCB天线需要特殊工艺处理吗?