This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助,CC430F5137接收数据问题

两块板,无线通信成功(依据是CRC校验OK点亮LED),现在想把接收到的数据取出来发送到串口,串口部分带有自动回显,应该是没有问题的,

问题是,A板从串口接收数据通过无线发送到B板的时候,输入的是6个字节的“012345”,输出的是112个字节,而且其中看不到 30 31 32 33 34 35,

我想问,我应该怎么操作,才能取出想要的数据?部分代码如下。

/*******************************************************************************
**接收中断处理
******************************************************************************/

#pragma vector=CC1101_VECTOR
__interrupt void CC1101_ISR(void)
{
  switch(__even_in_range(RF1AIV,32))        // Prioritizing Radio Core Interrupt 
  {
    case  0: break;                         // No RF core interrupt pending                                            
    case  2: break;                         // RFIFG0 
    case  4: break;                         // RFIFG1
    case  6: break;                         // RFIFG2
    case  8: break;                         // RFIFG3
    case 10: break;                         // RFIFG4
    case 12: break;                         // RFIFG5
    case 14: break;                         // RFIFG6          
    case 16: break;                         // RFIFG7
    case 18: break;                         // RFIFG8
    case 20:                                // RFIFG9
      if(receiving)			    // 接收触发的中断
      {
        // Read the length byte from the FIFO       
        RxBufferLength = ReadSingleReg( RXBYTES );               
        ReadBurstReg(RF_RXFIFORD, RxBuffer, RxBufferLength); 
        __no_operation(); 		   
        // Check the CRC results
        if(RxBuffer[CRC_LQI_IDX] & CRC_OK)
        {                     
          delayms(10);
          PutString(RxBuffer);
          
        }
      }
      else if(transmitting)		    // 发送触发的中断
      {
        RF1AIE &= ~BIT9;                    // Disable TX end-of-packet interrupt                         
        transmitting = 0; 
      }
      else while(1); 
      ResetRadioCore(); 
      InitRadio();
      Strobe( RF_SRX );
      // trap 
      break;
    case 22: break;                         // RFIFG10
    case 24: break;                         // RFIFG11
    case 26: break;                         // RFIFG12
    case 28: break;                         // RFIFG13
    case 30: break;                         // RFIFG14
    case 32: break;                         // RFIFG15
  }  
  __bic_SR_register_on_exit(LPM3_bits);     
}


/*******************************************************************************
**串口中断处理
*******************************************************************************/
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
{
  switch(__even_in_range(UCA0IV,4))
  {
  case 0:break;                             // Vector 0 - no interrupt
  case 2:                                   // Vector 2 - RXIFG
    while (!(UCA0IFG&UCTXIFG));             // USCI_A0 TX buffer ready?
    UCA0TXBUF = UCA0RXBUF;                  // TX -> RXed character
     ReceiveOff();
     receiving = 0;
     Transmit( (unsigned char*)UCA0TXBUF,sizeof UCA0TXBUF);
     transmitting = 1;
    break;
  case 4:break;                             // Vector 4 - TXIFG
  default: break;
  }
}