你好,我将rfEasyLinkEchoRx rfEasyLinkEchoTx 两个例程导入launchpad后,TX一直绿灯在闪,RX一直红灯在闪,我看了例程里面的readme文件,符合Example Usage的第一个,请问这是一直在发送数据包吗?怎么感觉不太对。。。。。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我将rfEasyLinkEchoRx rfEasyLinkEchoTx 两个例程导入launchpad后,TX一直绿灯在闪,RX一直红灯在闪,我看了例程里面的readme文件,符合Example Usage的第一个,请问这是一直在发送数据包吗?怎么感觉不太对。。。。。
是一直在发数据包,readme里原文:
The user will require two launchpads, one running rfEasyLinkEchoTx (Board_1), another running rfEasyLinkEchoRx (Board_2). Run Board_2 first, followed by Board_1. Board_1 is set to transmit a packet every second while Board_2 is set to receive the packet and then turnaround and transmit it after a delay of 100ms. Board_PIN_LED1 on Board_1 will toggle when it's able to successfully transmits a packet, and when it receives its echo. Board_PIN_LED2 on Board_2 will toggle when it receives a packet, and then when its able to re-transmit it (see [figure 1]).