This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F程序移植从7*7封装到4*4后,程序无法下载。

Other Parts Discussed in Thread: CC2640R2F

CCS无法顺利下载程序,但是RF_flash_programmer可以识别板子并下载或擦除程序,但是程序不运行。是否说明板子硬件无问题。

CC2640R2F程序移植从7*7封装到4*4后,程序无法下载。CCS 下载到最后一点跳转在线debug时出错,报错如下

Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: GEL Output: Board Reset Complete.
Cortex_M3_0: Can't Run Target CPU: (Error -2134 @ 0x0) Unable to control device execution state. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.48.0)
Cortex_M3_0: JTAG Communication Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.48.0)