This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc3200开发板WIFI部分AP和station模式无法使用的问题。

Other Parts Discussed in Thread: CC3200, UNIFLASH

1、cc3200开发板正常接电后,红灯闪了三下,OOB例程正常运行了,可是用手机和笔记本电脑都没办法搜到热点;

      tera term上显示信息:

               *************************************************
                           CC3200 Out of Box Application
               *************************************************

                            Manufacturer ID: 0x5449
                            Device ID: 0x67
                            Configuration register value: 0x7480
                            CHIP ID: 0xf8
                            [NETAPP EVENT] IP Acquired: IP=192.168.1.1 , Gateway=192.168.1.1

                           Connect to : 'mysimplelink-4430CC'

这是正常的结果,可是搜不到热点,无法连接它。

我尝试着格式化了cc3200,并且烧录了在官网上下的服务包,又重新烧录了OOB例程,但问题依旧。

2、运行Wlan-station例程中修改了ssid、安全类型和密码,无错误,但是无法连接到接入点。

不知哪位大神能帮我解决一下!

  • 请问你的开发板是TI的开发板吗?还是你们自己的

  •  你好,这个开发板是我们在TI官网上购买的。

  • 注意Pin脚的选择

    NoteNote: : In case device is coming up as AP (Jumper on VCC+P58) check Terminal prints to get to know device's AP name.

    Overview

    This Application demonstrates Out of Box Experience with CC3200 Launch Pad. It highlights the following features

    1. Easy Connection to CC3200 Launchpad
      • Direct Connection to Launchpad by using CC3200 device in Access Point Mode(Default)
      • Connection using TI SmartConfigTechnology
    2. Easy access to CC3200 Using Internal HTTP server and on-board webcontent
    3. Attractive Demos
      • Home Automation
      • Appliance Control
      • Security System
      • Thermostat

    For more information please refer CC32xx Quick Start Guide

    Usage

    • The CC3200 Launchpad comes with all the required content flashed to run the application
    • Refer Quick Start Guide for detailed information
    • In case user flashed other SDK applications and need to download the out of box content again, follow below steps
    • Open <cc3200-sdk>\examples\out_of_box\html\out_of_box.ucf session file in Uniflash.
    • Flash the files to the device. Detailed instructions at Uniflash User Guide.
    • Run the reference application
      1. Run From IDE (IAR/CCS)
        • Open the Example Project as mentioned in the <cc3200-sdk>\docs\CC3200-Getting Started Guide.pdf
        • Build and download the application to the board
      2. Run From Flashed Binary
    • Connect to CC3200 device as mentioned in Quick Start Guide, You will see below main page on your browser 

    NoteNote: : In case device is coming up as AP (Jumper on VCC+P58) check Terminal prints to get to know device's AP name.