1.板子用USB连接PC,打开PC识别的串口,可以看log。
2.用GCC编译wlan_station_demo生成bin,短接SOP2,然后用uniflash先format, 选择1MB容量,然后烧写wlan_station_demo到SPI FLASH。
3.移除SOP2,reset之后程序运行,log如下:
*************************************************
CC3200 WLAN STATION Application
*************************************************
Host Driver Version: 1.0.1.13
Build Version 0.0.0.0.31.0.0.0.0.0.0.0.0
Device is configured in default state
Device started as STATION
[WLAN EVENT] STA Connected to the AP: ,BSSID: 0:0:0:0:0:0
[NETAPP EVENT] IP Acquired: IP=192.168.43.220 , Gateway=192.168.43.1
Connection established w/ AP and IP is aquired
Pinging...!
Device pinged both the gateway and the external host
WLAN STATION example executed successfully
注意,刚运行是还没连接到wifi时,红色LED闪烁,连到wifi后,三个LED灯常亮。
wifi的名称是在common.h里面修改为自己的wifi名称和密码即可。