TI的工程师,你好!
CC3200 AP模式下
1.怎么实现连接多个设备
2.怎么主动断开连接?
能否提供些思路?需要用到哪些API?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前CC3200是configuration AP,只是支持一个设备连上了做配置,不支持多台设备。
TI后面会有CC3200的升级芯片推出,最大可支持4个Station,请关注TI的官网资料介绍。
请问现在最新的芯片支持多个设备连接了吗?哪里可以查到最新的信息?
目前的芯片还是支持一个设备连接,最新的信息就是在ti.com上搜索CC3200就可以获得了。
请告知具体查询位置。我在ti.com上搜索CC3200读了器件描述,没有找到哪个位置有写能接入1个设备或者4个设备。现在我们想开发接入4个设备的产品,因此需要确认该器件是否升级过,最好得到官方的数据。谢谢。
如果要支持连接4个设备,建议使用CC3200的升级芯片CC3220,这颗芯片可以支持4个Station的连接,而且还有CC3220SF版本内置了1M的Flash空间给客户使用
并且新的CC3220支持IPv6。
http://www.ti.com.cn/product/cn/CC3220?keyMatch=CC3220&tisearch=Search-CN-Everything
你好,
官方的评估板大约会这三月份陆续供货,全新的CC3220评估板,最新的进展请关注TI官方网站信息。