您好,The BQ25895 can provide up to 5A of output current draw (3A at battery and 2A at SYS is therefore okay), but only with an adequate input supply.
The device will enter thermal regulation where charge current is reduced when the chip temperature is too…
Part Number: BQ25895M Other Parts Discussed in Thread: BQ25895 你好!BQ25895是可以同时检测芯片本身温度,也可以通过TS脚检测电池的温度是否有异常?对吧,目前有个问题,我们TS脚NTC检测功能没有使用,我按照规格书上采用两个10K的分压后连接到TS脚的,VBUS输入采用12V,这样的话有个问题REGN电压是6.1V左右,TS脚是3.0V左右,有时候TS脚会偏低可能会低于2.9V,这样是不是容易引起芯片误判,以为TS脚温度不正常,比较接近Hot…
Part Number: BQ25731 Other Parts Discussed in Thread: BQ25622 , , BQ25895
我发现高压快充芯片,支持typec cc协议的都是buck boost芯片,只有支持dp dm才有单节电池高压快充芯片
想要咨询一下为什么只有buck boost芯片支持cc,有没有支持cc协议的单节快充芯片
感谢
Other Parts Discussed in Thread: BQ25622 , BQ25895 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。 https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1238896/bq25622-votg-and-vbus 器件型号: BQ25622 主题中讨论的其他器件…