请看是不是下面的原因引起的 ?
4.3 Debugging with MMWAVE_L_SDK
The code built for the xWRLx432 devices automatically runs with low power modes enabled. The low power modes do not allow for stepping through the code or setting breakpoints. To use the full debug capabilities…
Part Number: TMS320F280039C Other Parts Discussed in Thread: C2000WARE , SYSCONFIG 1.我按照clb user guide 进行设置了,目前出现了以下问题,目前别的文件生成都正常,但是没有vcd文件,同时也没有simulation文件夹
2.编译的结果是
"C:\\ti\\ccs1240\\ccs\\utils\\bin\\gmake" -k -j 16 clean -O DEL /F "syscfg…
Part Number: LP-MSPM0C1104 hi, experts:
Does the evaluate board need special USB cable or did I miss any jumpers? I can't download or debug with LP-MSPM0C1104 in CCS Theia 1.3.1 as attached screenshots.
Bill
Part Number: AM62P Hello TI team
When I was debugging, the following issue occurred: "Texas Instruments XDS100 USB Debug Probe0/CS-DAP0: Target must be connected before loading program." The starting position was 0x00000044. I am currently stuck with…
Part Number: PROCESSOR-SDK-J721E Question 1: Can the XDS100V2 debugger be used to debug the J721EXSKG01EVM? There is an interface mismatch between them; the XDS100V2 has a 14-pin interface, while the JTAG interface on the J721EXSKG01EVM is 20 pins. Is it…
Part Number: AM62P
Hello ti team When I was burning the program, I encountered an error message, "Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable…
Hello,
The error might be related to memory access issues. Check if there are any out-of-bounds memory accesses or pointer-related problems in your code.
Regards,
Gary