Part Number: DLPC350 Other Parts Discussed in Thread: DLP4500
原因:DLP4500方案(DLPC350ZFF),由于 M29DW128GL70N停产买不到料,更换为 MT28EW128ABA1LJS-0SIT
问题:使用JTAG flash programmer烧录bootloader后,显示烧录成功,但无法启动,连接USB不成功。
请教下是否需要bootloader对此flash进行适配?还有其他问题导致? MT28EW128ABA1LJS…
1.指向没有例子,就是一个概念
数据对由handle和Value组成,关于数组内0,1认为是指向特定数据对的索引 比如说0指向的是handle,而1指向的是value,它们共同作为一个数据对
2. pDataList 的参数定义是和属性表有关
to read a Characteristic Value from a server 读取的是server端的
https://software-dl.ti.com/lprf/simplelink_cc2640r2_latest/docs/blestack…
Part Number: TPS546D24A Hi we want to use BMC to dynamically change the VR output to 1.8V , but the voltage output became 1.4V by reading the meter.
The command as below:
Pls kindly help to check the command as below,
i2cset -y 2 0x1c 0x24 0x0466 w ;…