你好,参考下工程师的回复:
With AC input it works as a PFC input stage. It boosts the input volt to generate a higher DC bus volt and shapes the input current. This is average current mode control (ACMC) AC/DC boost.
But for DC input, it will be the same except that…
Part Number: DLPC350 Other Parts Discussed in Thread: DLP4500
原因:DLP4500方案(DLPC350ZFF),由于 M29DW128GL70N停产买不到料,更换为 MT28EW128ABA1LJS-0SIT
问题:使用JTAG flash programmer烧录bootloader后,显示烧录成功,但无法启动,连接USB不成功。
请教下是否需要bootloader对此flash进行适配?还有其他问题导致? MT28EW128ABA1LJS…
We do not have schematic examples for MSP-EXP430FR6989 connect with TCAN4550-Q1 in Official public resources.
If you want to know TCAN4550 how to connect to MCU or processor. such as SPI> CAN bus.
We have total solution of reference designs on TCAN4550…
感谢您对TI产品的关注! 关于你的咨询,IWR6843AOPEVM 不支持直接和DCA1000配合。 而xWR6843ISK和IWR6843ISK-ODS,支持和DCA1000直接配合。
mmWaveICBOOST你可以把它看作一个扩展接口的底座。 下面是它的功能。
1.2.5 MMWAVEICBOOST • Hosts starter kit using two 60-pin high-density (HD) connector for the high-speed ADC data over CSI…
您好
Transient model只能做the simulation of some transient functions, cannot measure loops.
您可以用 Average Model。
这有篇相关的技术文章,您可以看看。
www.ti.com/.../sluaa51.pdf
我帮您查了一下TI的教程,有一个视频简单介绍了一下,您可以看看。
PSpice for TI: AC Sweep Analysis | Video | TI.com