Part Number: PROCESSOR-SDK-J721E Question 1: Can the XDS100V2 debugger be used to debug the J721EXSKG01EVM? There is an interface mismatch between them; the XDS100V2 has a 14-pin interface, while the JTAG interface on the J721EXSKG01EVM is 20 pins. Is it…
您好
您的console里面有两个报错-260和-1170。
-260解释如下
可以尝试升级firmware,方式如下
https://software-dl.ti.com/ccs/esd/documents/xdsdebugprobes/emu_xds110.html
-1170解释如下
This error is caused by the inability of the JTAG debugger to access the DAP or one of its ARM subcores…
Under the Smart RF configuration panel, the communication between 1310 and 1310 is normal, but the communication between 1101 and 1101 does not seem to work. I found before that when CC1101 connects to RF studio and executes the send data command, only…
Other Parts Discussed in Thread: AM2432 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。 https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/1308122/does-the-xds-debugger-uses-the-boot-code 主题中讨论的其他器件…
Haoxiang Hu 说: 程序就被擦除了,
有没有连接调试器读一下FLASH中的内容?程序成功烧录到FLASH中以后下电也是不会丢失的,程序大概率只是没有运行起来。
CLB可以看作是集成到C2000中的一个FPGA/CPLD,代码只是起到配置的作用;
没有运行起来的原因具体其说起来有很多,但是总结起来大多数都与时序有关。
CCS/TMS320F28379D: Urgent: CLB not work when running from flash :比如这个问题的解决方案是在读取编码器前增加延时…
Other Parts Discussed in Thread: TMDS243EVM 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。 https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/1303793/speed-up-xds-100-debugger-clock-speed 主题中讨论的其他器件…