Part Number: LM5163 我现在的电路需要一组±90V的电源,我的正电源90V使用了LM5022MM从24V升压可以得到。负电源90V现在没有方案实现,所以需要请教一下:LM5163是否可以从24V变成负90V?或者是否有其它方案可以实现负90V输出?(因为空间有限,反激式电源可能放不下,当然如果有小型化的方案也可以考虑),负载功率在10W附近。
Part Number: INA226
故障描述:
我在板子供电但是并没有输入电压的时候,即VCC为0V的时候,对INA226进行通信,但是INA226反馈数据却是上面那个图的内容,4FF和2FF,就算我给VCC提供什么样的电压,电压反馈数据都不改变,电流的也一样,刚开始我以为是芯片的问题,但是我尝试用我的另一块单片机对其进行扫描,扫到了INA226读取和写入的地址,因此INA226我确信是在工作的,I2C总线上拉电阻在OLED上,我在INA226的scl和sda没有接上拉电阻,而我的OLED0…