Part Number: TMS320F280039C Other Parts Discussed in Thread: TMS320F28035 , 在TMS320F28035的勘误表中,说明了在ADC转换过程中,SOC有可能出现转换不准确的问题,请问在 TMS320F280039C中,会出现这样的问题吗?
Part Number: INA226
故障描述:
我在板子供电但是并没有输入电压的时候,即VCC为0V的时候,对INA226进行通信,但是INA226反馈数据却是上面那个图的内容,4FF和2FF,就算我给VCC提供什么样的电压,电压反馈数据都不改变,电流的也一样,刚开始我以为是芯片的问题,但是我尝试用我的另一块单片机对其进行扫描,扫到了INA226读取和写入的地址,因此INA226我确信是在工作的,I2C总线上拉电阻在OLED上,我在INA226的scl和sda没有接上拉电阻,而我的OLED0…
Part Number: ADC3663 Other Parts Discussed in Thread: TXS0108E-Q1 ADC3663的SPI配置管脚连接至FPGA时遇到IO电平不匹配问题。FPGA的IO是2.5V CMOS电平,ADC3663是1.8V CMOS电平,但是3663的SPI的IO内部有上拉或者下拉21K电阻,目前使用的双向电平转换芯片是TXS0108E-Q1。3663的SCLK和SDIO管脚信号电平不满足要求,会出现类似如下波形:
ADC内部的下拉电阻是无法改变的…
Part Number: TMS320F28335-Q1 Other Parts Discussed in Thread: TCAN4550-Q1 您好,想问一下F28335这款芯片SPI模块是不是只能发16位数据?不能发32位数据
我在配置TCAN4550-Q1芯片地址的时候,发现该芯片寄存器地址都是32位的