Part Number: DRV8871 Other Parts Discussed in Thread: DRV8870 , DRV8873 , DRV8243-Q1
请教一下,DRV8871的输入端IN1、IN2输入的是静态数据,例如IN1=1(高电平)、IN2=0(低电平),持续时间为200ms,之后IN1=0,IN2=0,周期是2秒;测试发现,DRV8871的OUT1、OUT2输出为PWM波形,占空比为50%,持续时间是200ms(与IN1=1,IN2=0持续时间一直),请教一下,为什么OUT输出是PWM…
Part Number: TPS40200-HT 输入:40~50V DC ;输出24V/100mA、30V/100mA两种。
典型电路如下图所示,电感选择铁硅铝材质,电阻电容均选择200度以上器件,。频率70kHz~200kHz均调试过。
在200度环境下拷机试验,输出均有不同情况下降,其中24V电源输出下降2V多,30V电源输出下降3~4V,datasheet显示内部基准是随温度升高上升的,高温下请问是什么原因导致此情况?
Part Number: BQ27Z746 如图,充电mos管关闭时,充电电源有一个波动电压,高于B+*2(B+最高电压为3.6V,铁锂电池)电压,通过此路径进入bq27z746,烧坏IC;R9和R10修改为1K后,此现象消失;能否帮忙评估一下,修改此电阻是否会有其他影响?我们也测试了部分样品,暂时没有发现异常。
Part Number: LMP91000EVM Other Parts Discussed in Thread: LMP91000 您好,我配制了各种浓度的铁氰化钾溶液,理论来讲,通过LMP91000测得电流绘制出的循环伏安曲线应该有氧化峰和还原峰。但是我测得的结果只有氧化峰,请问是否是设置上有什么问题?谢谢