先附上电路图

图中最前面的电压为5V 最后一级为15V
后面一个7001没有使用前级pro放大器
第一个7001输出电压为1V的有效值 且直流电压分量在-5mv到20mv之间波动
后面一个7001的放大我设置为5倍 实际输出有效值为4.5v的有效值 直流电压为-600mv
输出波形不错
但是芯片会发热 虽然不是很热 但是我感觉不正常
请各位老师解释一下原因
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 最后一级需要这么大的有效值?4.5VRMS对应的峰峰值大约有13V了,最后一级的输出电压太大。试试加负载后是否还是这么热。
2. 第二级的600mV直流有些可疑,按照之前帖子所述,DC offset被校准掉了,输出端按说不应该有这么大的直流成分。