由于需要电压隔离采样,采用了amc1200+LM258的形式,amc1200采用560欧与480K的电阻分压,将200V的电压分到250mV以内,输入到amc1200。amc1200后面输出采用差分放大电路,将amc1200输出电压放大1.5倍,送入到DSP的AD口。实测发现,直流电压在50V以内时,LM258输出电压为0.7V始终不变,这样就无法检测50V以内的电压。不知道是怎么回事?amc1200采用5V隔离电源,LM258同样采用5V供电。请问原因在哪里?该如何解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
请注意,你的LM258用的也是单电源供电。不知道你电路什么样的,需要注意电路AMC1200的输出共模电压和LM258的共模电压问题。可以考虑用TI的仿真软件TINA来做仿真: 链接如下:
http://www.ti.com/tool/TINA-TI?keyMatch=TINA&tisearch=Search-EN-Everything
谢谢
你好,我算了一下,单纯考虑LM258的输入失调电压影响不会这么大的,你电路贴出来看看,谢谢。
如果是单电源5V供电,建议使用LMV358,轨到轨输入输出的运放。普通的运放输出电压比电源会低1-2V。