Other Parts Discussed in Thread: LM258, AMC1200, LMV358
由于需要电压隔离采样,采用了amc1200+LM258的形式,amc1200采用560欧与480K的电阻分压,将200V的电压分到250mV以内,输入到amc1200。amc1200后面输出采用差分放大电路,将amc1200输出电压放大1.5倍,送入到DSP的AD口。实测发现,直流电压在50V以内时,LM258输出电压为0.7V始终不变,这样就无法检测50V以内的电压。不知道是怎么回事?amc1200采用5V隔离电源,LM258同样采用5V供电。请问原因在哪里?该如何解决?