Other Parts Discussed in Thread: OPA551, OPA547, BUF634
我需要一个电压跟随器,但是它不是针对交流信号的,而是可以针对直流电压信号的,我需要一个电压输出能从0V~12V,且输出电流能超过200MA的运放或者功率运放都行,可以用作电压跟随,有这种型号?有的话,它的接线方式跟普通电压跟随器是一样的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以采用这种高速buffer,G=1,BUF634,输出电流能达250mA,不知是否满足你的需求。
OPA551可以做电压跟随,单位增益稳定。shanping chen 说:可以用作电压跟随器?这些器件