This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA309传感器激励电压问题。

Other Parts Discussed in Thread: PGA309, PGA308, PGA300

准备使用PGA309设计一款压力变送器,查询得知PGA309压力传感器接口上的传感器激励电压在VREF为4.096V时最大为3.4V,而我这边电路要求VREF为2.5V,所以激励电压只有2.075V。但我们的压力传感器激励电压要求为5~10V,请问这里有没有已有的解决方案?我的电路中电源使用可以灵活,但必须尽量少的引入噪声。

  • TI的工程师能不能给个回复?

  • 从你处描述看,前端要接入应变片式传感器?此类传感器灵敏度较小,因此需要较大方法倍数。不确定你的应用需要温度补偿、非线性校准功能吗?如果上述不是必须的话,PGA308也可以考虑。

    另外新进推出的PGA300或许也可以考虑。

    如果还有问题,请留下你的邮件地址,我可以单独发邮件给你

  • 你好,我这个项目前端是接入应变片式传感器,灵敏度范围在0.5~2.5mV/V。为了达到放大要求,PGA309后面加了放大电路。现在问题是输出噪声电压偏大,测试发现噪声出在PGA309部分。而且Output Stage Gain不为2后噪声更加明显,Output Stage Gain设为3.6后PGA309输出噪声跳动在2mV以上。现在传感器激励电压VExc为2.5*0.83V,能否放大VExc而使用小的Output Stage Gain。还有噪声问题有没有好的解决方法。

    期待讨论

    我的邮箱地址:daiqb@bozhon.com

  • PGA309内部有自稳零放大器,会有调制噪声,通过合理设计滤波器截止频率可以规避这一问题。 如此链接地址,http://www.ti.com/lit/an/sboa110a/sboa110a.pdf

  • 设计滤波器截止频率是指调节Vout与Vsj之间的电容吗,噪声问题没有得到解决,即使按照截止频率1KHz来设置噪声问题依旧严重,而我的系统带宽要求5KHz。PGA308这个问题会好一点吗

  • 我先看看你的电路。另外最好能用示波器看看输出,确认是噪声问题。两级放大所使用的增益分别是多少?还有一个问题,温度补偿与非线性校准你处是必须的吗?

    也可以发邮件给我.