Other Parts Discussed in Thread: OP07
我的电路是按照这个电路连的,但是OP07是双电源供电
我输出时最小有1点多V,然后输出到2点多V时,输出电平会一下子跳变到4点多V
不知道是什么原因,求助,多谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OP07
我的电路是按照这个电路连的,但是OP07是双电源供电
我输出时最小有1点多V,然后输出到2点多V时,输出电平会一下子跳变到4点多V
不知道是什么原因,求助,多谢
跳变是不是你滑动变阻器的原因?输出4V多的时候,有没有量下同相输入端电压,看输出和输入的比例关系是否还是正常的。
你好,两者的比例关系也不正常
一开始我信好增大,他输出电压变化很小是0.000的级别变化,
等到我输入电压到1V左右程度的时候,他输出变化才开始变化的比较大
OP07不是轨到轨输入输出的。从你图上看,如果是单电源供电的,输入太小时,芯片是不会正常放大的。
你把输入调高点,看是不是正常2倍放大输出,如果比例正常,说明就是上面讲的问题。
不是轨至轨芯片的话,对信号输入范围有要求,单电源供电时候,在接近GND电平附近的信号是没法正确处理的,因此需要看下OP07输入共模电压范围。Haojie Xu 说:输出时是输入大的时候比例是对的,小的时候就不对了
这个还和是不是轨到轨芯片有关啊