This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6550: 关于LMH6550输出电流能力,线性输出电流和短路电流的差别

Part Number: LMH6550

您好,在LMH6550的规格书中,提供了线性输出电流(VOUT=0)以及短路电流(Output Shorted to Ground VIN=3V Single-Ended)两种指标。我想知道的是:

1.线性输出电流的测试条件条件中的VOUT=0指的是差分输出Vout,dm=0V吗,也就是将OUT+与OUT-短接测试时的电流值?

2.如果不是上述情况,那这个指标是具体什么条件下的电流呢?为何叫做线性输出电流

3.短路电流的测试条件中提到的Output Shorted to Ground指的是短接到系统的参考地吗?比如对于±5V的电源情况,结合总条件G=+1来看,也就是VIN=3V,则输出悬空时OUT+=1.5V,OUT-=-1.5V。此时将OUT+和OUT-分别向0V短路,测到的电流就是此处标定的短路电流吗