设计使用了TI的D类音频功放TAS5630与TPA3250,电路参考了DATASHEET上的设计(BTL Application),但是只用了其中的一路输出;
1.上电后,即使没有输出,芯片发热量也很大;D类功放的发热量为什么会这么大?TI的DEMO也是这样吗,必需配合散热片使用?
2. 简单提高或降低PVDD VALUE(都在芯片定义范围内),对芯片的发热是否有影响?
3.不使用的输出通道,PVDD是否可以直接不接电源?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
建议参考我们评估板线路设计,如果有一路不用,PVCC还是接上比较好。如果只需要一个声道,也可以选用单声道的器件。
TPA3250: Signal Bandwidth up to 100 kHz for High Frequency Content From HD Sources
请问TPA3250有单声道的器件推荐吗?
原贴中关于发热的问题,请帮忙回复一下,感谢。