你好,我用VCA820 datasheet 23页Figure84搭出来的图检测,Rf和Rg分别为1K与200,测试电压为200KHZ、0.2mV的正弦波,增益理论上最大应该是10倍,现在最大只有2~3倍,但是增益随控制电压Vg的走势与datasheet中的基本一致,极度郁闷,求解中!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 0.2mV的输入是不是太小了?820的DC offset都已经在mV量级了。
2. 前端的50Ohm匹配会不会对信号有分压?
3. 建议先用TINA仿一下,看看频率响应。
原帖是0.2mV输入的正弦波,看来是笔误了。另外,你的供电电压是多少?
注意到你的运放输出端有一个50 Ohm的电阻,在实际电路中是把100 Ohm接到50 Ohm后面,然后把图23的Vout作为整个电路的输出?附上TINA仿真,从仿真结果来看,放大倍数大约在6.5倍,如果算上你输入端接50 Ohm匹配造成的0.5倍衰减,大约总的放大倍数是3.3倍。

建议你对照仿真电路图和仿真结果检查一下你的实物电路,看看原因是不是出在输入50 Ohm匹配分压和输入50 Ohm的分压上。