Other Parts Discussed in Thread: TAS5701, TAS5707
TAS5701做数字功放 我带的是8欧姆的负载,输出幅度在8 9VB的时候,就会出现有一段信号缺失的想象,看起来像保护的,可是电压 电流都正常,温度也没有问题,请问这是什么原因呢?大侠们。。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
手册第9页有个Ioc,4.5A,看上去像是过流了就把电流限制在4.5A。所以即使电压电流跟之前没太大区别,你也很难保证芯片没进入过流区啊。试试挂大一点的电阻负载,看看还有没有信号确实的现象。
如果可以使用I2C建议使用TAS5707。
对于出现问题后,请检查FAULT PIN 的状态。
另外确认OC_ADJ外部电阻是否是1% 18.2k,确保过流点正常。