Other Parts Discussed in Thread: OPA454, TPS55340
各位大神:
小弟最近碰到一个问题,我用OPA454做了一个简单的加法器电路:运放反相端接3V电压源和一个10K电阻,正相端接一个个幅值为0~3V的正弦波,负反馈回路上接一个10K电阻,则输出Vout=2*(Vdac)-3。目的就是将0~3V正弦波变成-3~3V的双向正弦波,该电路采用±34V供电(是考虑到后面的电路才采用这么高的供电电压),现在的问题是:当我使用两个开关电源给运放供电的时候,电路正常运行;但是当我使用升压芯片产生+-34V电压从而给运放供电时,运放的供电电压降为了+12V和-8V,我觉得原因可能是升压芯片的阻抗太大了(输出端有一个2.61M和100K电阻并联)从而形成分压,但是那个升压芯片电路是datasheet上给的推荐电路,不知道各位对这个问题怎么看?能不能麻烦给点指点,不胜感激!电路图如下所示: