OPA4376对电流传感器的输出信号进行调理,然后送给ADS7863转换。OPA4376为±2.5V供电,输入信号频率小于100Hz。
刚才看到一个贴说带宽为2M的运放不适合用在ADS7863的调理电路中,因为响应时间的缘故。请问OPA4376可以吗?它的增益带宽积为5.5M,会不会影响AD转换的性能?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看你要跑多快的采样率了。定下采样率后,对照着手册看一下采样时间,前端运放应该在采样时间内保证稳定的建立。最差的情况是前端的输出从-REF跳变到+REF,此时运放应该可以在采样时间内建立。另外,为了滤除噪声,前端运放通常会加一个RC低通滤波,这也会恶化速度(如手册图41所示)。建议在TINA里把前端运放电路和ADC的输入等效电路(如手册图1,因为已经写了RSW=50Ohm所以仿真时SW可以去掉,保留50Ohm电阻即可)放在一起仿一下,看看前端输出从最小跳变到最大时,运放的建立时间能否在ADC的采样时间内稳定。
分析了下电路,应该差不多。ADC每通道的采样率最大为150KHz左右,运放的输入信号频率最大为200Hz,且不会出现阶跃变化。OPA应该跟得上。