LM393在正负输入差模电压小于一定程度时,输出呈线性。举例说明,+端输入2V,-端输入1.9V,按常理输出在外部有上拉5V的情况下,输出为5V,但是实际测量其实只有3V多,感觉内部的MOS管并没有饱和,导致输出呈线性。
我想了解下,lm393手册上哪个参数是表示正负输入压差大于多少值LM393可以正常工作,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM393在正负输入差模电压小于一定程度时,输出呈线性。举例说明,+端输入2V,-端输入1.9V,按常理输出在外部有上拉5V的情况下,输出为5V,但是实际测量其实只有3V多,感觉内部的MOS管并没有饱和,导致输出呈线性。
我想了解下,lm393手册上哪个参数是表示正负输入压差大于多少值LM393可以正常工作,谢谢
建议您参考下手册的8.2.2.1 Input Voltage Range,http://www.ti.com.cn/product/cn/LM393/description
看了下有个override voltage为100mV,但是我看了下,这个过驱电压影响的更多是时延,和输出饱和或者不饱和影响不大,请解释的更清楚些,谢谢。
如果同相端和反相端都在输入共模范围之内,那么输出结果两种情况:
(a) If IN- is higher than IN+ and the offset voltage, the output is low and the output transistor is sinking current
(b) If IN- is lower than IN+ and the offset voltage, the output is high impedance and the output transistor is not conducting