Other Parts Discussed in Thread: OPA551, OPA552, OPA454
Hi:
输入为0~12.5V的直流模拟量,想增益放大4倍,输出0~50V;
输入-10V~10V的直流模拟,想放大2倍,输出-20~20V;
输入0~10V的直流模拟,想将其缩小,使其输出0~150mV;
以上输入信号均按低频处理(不需要考虑带宽),以及对于选择的运放iC的供电电压值最好是常见的。
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi:
能帮助提供下完整的方案吗?
Thanks
运放选型不仅仅只考虑输入共模电压和输出电压,还要考虑带宽,工作电压,失调电压。
你好,信号就是低频的,工作电压以及失调电压可以先不考虑,现在就是想要的是几个方案,然后我可以自己权衡其余的因素。
你好,超过50V的可以先放着,那么另外两个的方案你有什么好的办法吗??或者你可以将如何在TI官网查询目标放大器的方法告诉我。谢谢