最近做一个EQ均衡器电路,用NE5532搭建。电源为单电源,由220V转18V开关电源适配器(成品)提供,接上EQ电路带负载之后测得纹波Vrms约40mv左右,偶尔波动到60mv;示波器看峰峰值在100+mv,有尖峰噪声,在峰峰值在200mv左右;NE5532偏置电压由两个100K电阻分压得来。音频EQ电路图在附件,VR1、VR2没接。在把EQ均衡器电路后级断开、输入接地的情况下,在T6、T7 Testpoint测得纹波Vrms约10mv左右(VR3、VR4、VR5、VR6滑动变阻器调至中间)。
已经尝试过把C37和C23并联上1000uF的电解电容,有小许改善但是还解决不了EQ电路输出噪声大。尝试把18V开关电源适配器更换成线性电源,EQ电路输出噪声Vrms小到200uV以下,应该是电源问题。然后尝试改成负电源,负电源由TPS63700 DC-DC转出-18V,纹波在Vrms 30mv左右,结果EQ电路输出纹波Vrms 20mv左右,反而更大。请问怎么才能减少EQ均衡器底噪大的问题呢?改成双电源理论上纹波应该会更小一些,但是实测没有改善,请问问题出在哪个地方呢?要求使用原来的18V开关电源适配器来作为电源,EQ电路输出纹波在1mV以下,最好在500uV以下,求各位指导一下该怎么改~
由于这个电路是由以前证实可行的电路由双电源改成单电源来的,且以前的电路电源纹波较小Vrms小于5mv。改用TL082会不会有改善呢?