This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

检测电流用哪款IC比较好,INA214如何?

Other Parts Discussed in Thread: INA214

目前项目中有需要检测最小为1微安的电流,想问一下使用INA214配合采样电阻能否实现,如果可以用INA214的话我该搭配多大的采样电阻比较合适?或者有其他更好用的方案?还请各位多多指点,详细说明。

  • 测量小电流最直观的办法就是串接电阻采集压降,根据采样电阻在电源线还是地线上可以再分为高边或者底边。1uA的电流的确够小,最大电流有多大?希望输出电压在那个范围?

    需要根据以上参数给出建议。

    除此之外,运放可以搭建为跨阻放大器形式,直接将输入小电流放大为电压信号,同样需要了解你处输入电流范围、期望输出电压值

  • 使用高侧测量,输入电流为2mA到1uA,输出电压为0到5V之间,能满足后端10位AD采样即可。