Other Parts Discussed in Thread: LM2903
请问LM2903 双比较器能接正负双电源么 ?看规格书,只标明最大VCC电压36V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM2903
请问LM2903 双比较器能接正负双电源么 ?看规格书,只标明最大VCC电压36V。
These devices consist of two independent voltage
comparators that are designed to operate from a
single power supply over a wide range of voltages.
Operation from dual supplies also is possible as
long as the difference between the two supplies is
2 V to 36 V, and VCC is at least 1.5 V more positive than the input common-mode voltage.
也可以双电源供电的哈。数据手册中第一页就有描述:Single-Supply or Dual Supplies