Other Parts Discussed in Thread: LM2902, TLV4172, TLV172, TINA-TI
原来用的是ADI的一个放大器是完全可以的,改用LM2902也是可以的,就是LM2902的精度差了,改用TLV4172但是新的问题来了,双电源+5V,-5V,5脚是基准2.5V,6脚是反馈端,7脚是输出,那么问题来了,7脚输出电压偏低,而且是可能是被肖顶了,2902都没这个问题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
+-5V供电的话,基准是0V就可以,设置2.5V,那么你的输入信号是多少?有可能输出饱和导致削顶。
另外,TLV4172是4个通道的TLV172,5脚不是基准引脚呢?
输入信号经过电阻接到6脚,基准是外部给的,TLV4172不是轨到轨吗,输出按说不会肖顶,用LM2902都没事,TLV4172输出7脚电压应该是受限制到了某个值,这个值离5V还挺远
TLV4172输出是轨到轨,我担心你把基准设置2.5V导致输出饱和。 双电源供电,输入信号在其共模电压范围之内,可以不用基准。
能否把完整电路图贴上来看下?输入是什么幅值的信号?
你好,
你的输入信号频率是多少?负载是多少?
放大器的输出电压,还需要考虑信号频率和输出负载的影响
Best regards,
Sulyn Zhang
信号频率100KHz,输出经11KΩ接到4172做的 跟随器的同相输入端,跟随器同相输入端的电压超过2.5V会不会被肖顶,数据手册写的是(V+) – 2
你好,
这个是放大器输入共模电压范围,削顶不会的。基于你提到的这个信号频率和负载情况,正常应该不会出现输出电压削顶的问题。另外,你Vs这个反馈信号接到哪的?
Best regards,
Sulyn Zhang