INA226的Alert引脚什么情况置0,提示master有保护,还有在什么情况下Mask/Enable Register(06H)的D15-D12置1
Shunt Voltage Over-Voltage
SUL: Shunt Voltage Under-Voltage
BOL: Bus Voltage Over-Voltage
BUL: Bus Voltage Under-Voltage
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
datasheet中对这部分讲的还是挺详细的,简单来说,就是测试的measured shunt voltage电压超过Alert limit register设置的limit值时,Alert就会响应。
不好意思,Alert Limit Register (07h)怎么设置Shunt Voltage Over-Voltage/Shunt Voltage Under-Voltage/ Bus Voltage Over-Voltage/ Bus Voltage Under-Voltage这些保护点,这个iNA226与ina209不一样,像INA209可以设置寄存器Shunt Voltage Negative Warning(0Dh),写入保护点,请麻烦讲解一下
您可以参考手册的7.6.7 Mask/Enable Register (06h) (Read/Write)
这几个过压,欠压点是客户自己设置的,比如bus voltage范围为0~36V,那么可以自己可以设置一个过压点,欠压点,比如设置18V就为欠压,37V就为过压。
需要注意的是,在配置 Alert Limit 寄存器时,不是直接将电压值转换为16进制就是寄存器的值,有个关系式,就是寄存器value=1.25mV*电压。
举例,我们设置18V为欠压,并不是直接配置Alert Limit Register为0X0012.
实际是:18V/1.25mV=14400.那么Alert Limit Register应该为0X3480=14400*1.25mV=18V.
你好,这个配置时序呢,如果我配置欠压点,是不是应该配置06H中的 的某一个点,再配置07H的值? 是这样的吗?