This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3886实验现象解析

Other Parts Discussed in Thread: LM3886

我是根据手册上搭的电路图,如下图。

条件:1、输入正玄波50khz,6vpp;2、V+=12V,V-= -12V;3、8欧负载;

现象:调节滑动变阻器Rin,使输入PIN10的信号为1VPP,此时输出正玄波50khz,21VPP,Irms=0.217A,这个情况基本是正确的。

但是,当我再次调节Rin,使输入PIN10的信号慢慢大于1VPP,此时输出的波形就慢慢变成矩形了,峰峰值和交流电流有效值也基本上不再增加,这个时候需要增加输入电压将输出波形慢慢调成正玄波。

问题:1、这种想象肯定是有原因的,变成矩形波貌似是一种失真,我想知道这种想象的具体原因;

2、根据功率计算公式,我是应该用峰峰值x交流电流有效值,还是峰峰值/2 x 交流电流有效值;

3、手册的第23页有个设计的例子,给的输出条件是40W,负载4欧,然后根据手册 给的公式计算Vo和Io,他计算的结果是Vo=17.9V,Io=4.5A,这根据功率计算公式,VxI的值远远大于了40W,这是为何?