Other Parts Discussed in Thread: INA2332
本人用INA2332放大信号,由于由负信号输入(几百毫伏脉冲信号)。所以用了正负5V电源,然后好像IC就烧了(V+和V-导通了)。应该是可以用正负电源的吧。还有就是8脚和14脚的shutdown脚是干什么的。是输入信号还是输出信号。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: INA2332
本人用INA2332放大信号,由于由负信号输入(几百毫伏脉冲信号)。所以用了正负5V电源,然后好像IC就烧了(V+和V-导通了)。应该是可以用正负电源的吧。还有就是8脚和14脚的shutdown脚是干什么的。是输入信号还是输出信号。
它的供电电压范围为2.7V到5.5V,双电源供电的话就是+-1.35V~+-2.75V.所以+-5V供电肯定会烧啊。
shutdown引脚是用来使芯片进入低功耗状态的,通常在一些便携式应用中,当器件不会一直处于使能状态时,可将其进入休眠模式。
刚刚用-1伏 和+3伏供电 为啥还是烧了。伤不起啊 烧了5片了。范围不是到5.5V呢吗 我才4V啊
同
http://www.deyisupport.com/question_answer/analog/amplifiers/f/52/p/128132/357775.aspx#357775