Other Parts Discussed in Thread: OPA695
你好!请问三个OPA695芯片并联,放大倍数设定为+8,并且用芯片的最大电源轨供电,这样可以把频率做到270MHz,并在带50Ω负载时输出5.7Vpp的幅值吗?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OPA695
你好!请问三个OPA695芯片并联,放大倍数设定为+8,并且用芯片的最大电源轨供电,这样可以把频率做到270MHz,并在带50Ω负载时输出5.7Vpp的幅值吗?谢谢!
OPA695的最大输出幅值为+-4.2V。
能否说下你的应用,单片OPA695使用,当G=8时的带宽为450MHz,输出最大也能到达+-4.2V。
你好!我是用这个芯片来做2015年电子设计竞赛放大器题的最后一级电路的。您给出的是OPA695芯片手册上的数据,但是我实际做的单级的测试条件和效果是:测试条件:单片OPA695,G=+8;用+-6.5V供电。测试结果:低频输出0.8Vpp以下时,频率可以达到300M以上;使低频输出1Vpp以上时,在100M以后就会失真。
根据题目的要求,单片OPA695是无法输出11.3Vpp幅值并且达到270M频率,所以我采用三片并联的形式。采用+-6.5V供电,发现输出11.3Vpp是频率只能达到20M。所以,我想问这种方法行得通吗?谢谢!