Other Parts Discussed in Thread: OPA552, DAC7311
现在的电路形式如图片那样(附件里也有照片),一个OPA552正向放大(VCC=+30V,VEE=GND)输出到OPA552的VCC,一个OPA552反向放大(VCC=GND,VEE=-25V)输出到OPA552的VEE,因为三个OPA552构成一路,板子上有很多路这样成本比较高,无法执行。现在希望TI工程师能推荐几个芯片能替代前级的两个正负放大的OPA552,后级的比较器还是用OPA552。
要求:
1、前级的两个正负放大的运放只是输出直流没有转换率和带宽的要求
2、正向放大的运放VCC=+30V,VEE=GND,能正常工作
3、反向放大的运放VCC=GND,VEE=-25V能正常工作
4、封装SOIC-8,最好是这个封装也可以不是。
5,跟DAC7311配合能正常工作。
6、价钱要低,最少也得比OPA552低。
谢谢!