Other Parts Discussed in Thread: OP07, LM358

是我OP07连接的不对吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
lize peng ,
你好,OP07最小供电是需要单电源6V或者双电源+3V/-3V,5V供电很可能不能正常工作,请注意。
如果回答了你的问题,请帮忙点击确认,谢谢!
Best regards
Sulyn Zhang
谢谢帮忙,不是电压的问题,是OP07电路R1和R3电阻值不一样,导致的,我都换成10K就输出值与输入值一样了,但现在出现一个新问题,我连实际电路用LM358,不管输入几V输出结果都是2.9V,,是不是我电阻的阻值选的不对呢?
对于LM358来说,因为不是轨至轨输出,所以输出达不到电源轨,您的输入是什么幅值的信号,供电电压5V的话最大输出3.5V左右。是不是输出饱和导致?
我的输入电压最大3.3v,实际输入测时是3V或者2v,1v