Other Parts Discussed in Thread: INA333
检测电流范围1-1000mA,采样电阻50mOhm,采用INA333低位检测,单电源供电(5.0V)。由于INA333输入电压需比地高0.1V(实测高于300mV)才能正常工作,。在2脚和3脚使用加法器叠加了1.25V电压。但是实际使用发现放大倍数有5%的误差(Rg=2.7KOhm,放大倍数在38到40之间摆动)。放在高位(输出5.00V)检测时(333电源电压5.5V)输入电压过高不能满足输入和电源电压余量导致放大倍数非线性(实测输出电压降到4.20V可以满足1000mA检测)。请问333是否不适合该情况使用?如果必须放在低位检测该选取什么芯片?