Other Parts Discussed in Thread: LM4991
LM4991 SOIC 封装 最大能驱动1.5W的扬声器
连接方式:音源为计算机前面板音频接口输出的音频信号,通过音频线(一分二音频线,分成左右声道),将任意一个声道连接到音频运放LM4991的输入端(4脚)。电源采用直流稳压电源供电5V,将5V稳压源的地与音频接口的地相连。运放输出接的是1W 8Ω的扬声器。运放设置为2倍的增益。
故障现象为:工作3~5秒后出现保护,扬声器停止放音,大概需要等待3~5分钟才能自动恢复正常,工作3~5秒钟,反复出现保护!通过示波器观察输入的音频信号电压峰峰值为120mV,有效值为25mV。不知道为什么输入这么小的音频信号还会出现保护,保护的时候芯片无发热现象(能够排除功率过大导致)。
。