Other Parts Discussed in Thread: THS4121, THS4521, THS4131
TI团队你好:
我对单端输入差分输出芯片THS4121有一些疑问麻烦解惑:
1、THS4121的单端输入的电压范围是多少?
2、单端输入 的电压可否是双极性的正弦波?我要采集的信号是有正负的正弦波
3、差分输出的信号一支跟输入信号幅值相位都形同,另一支幅值相同相位相反,对吧?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、THS4121的单端输入的电压范围是多少?
A: 单端输入电压范围为0.35V~VDD。
2、单端输入 的电压可否是双极性的正弦波?我要采集的信号是有正负的正弦波
A: 如果是双极性的,因为这款全差分是3.3V供电,需要将输入端加个偏置电路,保证其输入在其输入电压范围之内。或者可以看下THS4521这款,输入可达到负压轨。
3、差分输出的信号一支跟输入信号幅值相位都形同,另一支幅值相同相位相反,对吧?
A: 输出是差分信号,是的,幅值相同,相位相反。
忘了回复我的理解了,希望您能回复:
1、THS4121原来是单端供电的,不适合输入是双极性的信号;
2、你推荐的THS4521的双端供电范围是 ±2.25V,有点小,不如THS4131双电源供电可达 ±15V,
3、使用双电源供电的单端转差分放大器,是不是就可以输入双极性的正弦波信号了?